Real Time

PDCCH Transmission Configuration (Advanced LTE-A FDD Downlink)

In the Channel Setup node, select a DCI channel, then click the button in the Transmission Configuration cell to open the PDCCH Transmission Configuration dialog box. Click the Column Preset button to access a Closeddrop-down list that enables you to set the parameters for all PDCCH transmissions to the same value. Click the Radio Frame button to access a Closeddrop-down list that enables you to select a radio frame in which to configure the PDCCH. Click the Subframe button to access a Closeddrop-down list that enables you to select a subframe in which to configure the PDCCH. Select the All Subframes couple with subframe #0 checkbox to set the parameters for all subframes to the same values as those for subframe 0.

Frame

Subframe

State

Format

TPC PUCCH

Data

Data Size

RNTI

Search Space

Agg Level

Candidate

CCE Offset

Frame

Displays radio frame number.

Subframe

Displays subframe number.

State

Choice: On | Off  

Default: Off

Check (On) or clear (Off) to set the channel state.

Format

Displays DCI Format.

TPC PUCCH

Choice: TPC #0 (-1dB) | TPC #1 (0dB) | TPC #2 (1dB) | TPC #3 (3dB)  

Default: TPC #0 (-1dB)

Use the drop-down list to select the TPC PUCCH.

Data

Use the Data Source Selection dialog box to select PN9, PN15, or User Defined Bits to use for the data.

Data Size

Range: 1 to 100

Default: (depends on DCI Fromat)

Set the number of data bits to use.

RNTI

Range: 0 to 65535 (0xFFFF)

Default: 1 (depends on DCI #)

Enter a decimal value for the radio network temporary identifier (RNTI).

Search Space

Choice: Common | UE Specific

Default: UE Specific.

Select a search space from the drop-down list.

Agg Level

Choice: 1 | 2 | 4 | 8

Use the drop-down list to select an aggregation level.

Candidate

This parameter is set by the software.

CCE Offset

The control channel element (CCE) offset is determined by the CCE aggregation level as follows:

CCE Aggregation Size

(Num of CCE)

CCE Offset choices

1

0 | 1 | 2 |... N_PDCCHmax -1

2

0 | 2 | 4 |... N_PDCCHmax -1

4

0 | 4 | 8 |... N_PDCCHmax -1

8

0 | 8 | 16 |... N_PDCCHmax -1